我在用TLK3101作为3.125G光纤接口的收发芯片,在进行两个设备间的通信时,发现TLK3101的Rx_CLK 存在抖动和不连续的情况。但将两设备的时钟采用同源时钟,则不存在此问题。两个设备都是使用TLK3101作为光纤收发的串并转换芯片。请问这种情况是什么原因引起的呢??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在用TLK3101作为3.125G光纤接口的收发芯片,在进行两个设备间的通信时,发现TLK3101的Rx_CLK 存在抖动和不连续的情况。但将两设备的时钟采用同源时钟,则不存在此问题。两个设备都是使用TLK3101作为光纤收发的串并转换芯片。请问这种情况是什么原因引起的呢??
Hi Tony,
根据你的问题描述,初步判断是:当两设备采用不同源时钟时,此时在任一个设备上的RX_CLK和GTX_CLK即不是同源的,若你用示波器同时抓这两个波形,就会出现相位混乱现象。当采用同源时钟时,此时RX_CLK和GTX_CLK是同步的,你就会看到这两个时钟会比较稳定(相对相位关系固定)。
为了跟清晰理解你这个现象,请:
1)提供更详细的测试波形;
2)提供你现在电路设计中用到的时钟方案;
3)提供你测试的码流。
下面的链接供你理解类似SerDes的电路设计
http://www.ti.com.cn/cn/lit/an/zhca076/zhca076.pdf
xiexie.
Steven