Part Number: ADS1292
目前示波器测得以下PWM信号波形(频率为20~100KHZ,电压幅值设计为5V):主要是有大约500KHZ的纹波(幅值约占整体幅值的1/3),现在不想用示波器而是想要通过数据转换+STM32控制器,获知在PWM占空比变化1%时,整体波形的平均电压或有效电压变化量。

我想了解的是:
1、为了计算电压平均值或有效值,需要使用上MHZ采样率的ADC吗?
2、希望得到ADC推荐
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS1292
目前示波器测得以下PWM信号波形(频率为20~100KHZ,电压幅值设计为5V):主要是有大约500KHZ的纹波(幅值约占整体幅值的1/3),现在不想用示波器而是想要通过数据转换+STM32控制器,获知在PWM占空比变化1%时,整体波形的平均电压或有效电压变化量。

我想了解的是:
1、为了计算电压平均值或有效值,需要使用上MHZ采样率的ADC吗?
2、希望得到ADC推荐
我在下面链接找到了采样频率fs 与信号频率fi 的比值与采样误差的关系,如下截图
https://max.book118.com/html/2017/0709/121279333.shtm
看上面描述,通带上限分量的幅值为基频的1/3时,误差≤1%,fs/fi应不小于13;
也就是说如果在您的应用中通带上限是500KHZ,基频是100KHZ,误差≤0.5%的话,fs/fi的值大概在20,因为3/1.2=2.5,而1%除以2.5为0.4%,满足您的要求0.5%以内。
因此,这里关键是需要知道您需要采集信号的通带上限分量的幅值是多少?然后根据截图中表1估算出需要的采样频率。