This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1292: 使用什么样的ADC来采集PWM频率为100KHZ,纹波约为500KHZ的波形信号,并计算整体波形的平均电压或有效电压

Part Number: ADS1292

目前示波器测得以下PWM信号波形(频率为20~100KHZ,电压幅值设计为5V):主要是有大约500KHZ的纹波(幅值约占整体幅值的1/3),现在不想用示波器而是想要通过数据转换+STM32控制器,获知在PWM占空比变化1%时,整体波形的平均电压或有效电压变化量。

我想了解的是:

        1、为了计算电压平均值或有效值,需要使用上MHZ采样率的ADC吗?

        2、希望得到ADC推荐