主设备为280049
通过下方代码读取寄存器值,总是会读到0x7FFF的值,
但是如果在第25行 return sendCommand(OPCODE_NULL); 添加断点,则程序能正常读到寄存器值
请问是否在发送Command后需要等待一段时间才可以指定的应答数据?
uint16_t readSingleRegister(uint8_t address)
{
/* Check that the register address is in range */
assert(address < NUM_REGISTERS);
// Build TX and RX byte array
#ifdef ENABLE_CRC_IN
uint8_t dataTx[8] = { 0 }; // 2 words, up to 4 bytes each = 8 bytes maximum
uint8_t dataRx[8] = { 0 };
#else
uint8_t dataTx[4] = { 0 }; // 1 word, up to 4 bytes long = 4 bytes maximum
uint8_t dataRx[4] = { 0 };
#endif
uint16_t opcode = OPCODE_RREG | (((uint16_t) address) << 7);
uint8_t numberOfBytes = buildSPIarray(&opcode, 1, dataTx);
// [FRAME 1] Send RREG command
spiSendReceiveArrays(dataTx, dataRx, numberOfBytes);
// // [FRAME 2] Send NULL command to retrieve the register data
// registerMap[address] = sendCommand(OPCODE_NULL);
// return registerMap[address];
return sendCommand(OPCODE_NULL);
}