This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于ADS1256的应用与编程

Other Parts Discussed in Thread: ADS1256

1.能够对ads1256本身进行编程吗?还是只能通过MCU对其进行编程控制?

2.请问ads1256是否可通过其SPI接口接到SPI转RS485芯片上(MAX3140),使其转换后的数字量最终能够通过485接口输出?

  • 对“对ads1256本身进行编程”是什么意思啊?

    ADS1256可以理解为SPI的从设备,那么一定是要有SPI主设备与之相连。 spi的主设备一般是MCU

     

     

  • MAX3140如果能满足Figure 1. Serial Interface Timing 的时序要求也是可以的。

    不过还是建议用一个简单的MCU 去控制ADS1256,比如说MSP430G2440.

  • 非常感谢那你的回复!

    是这样的,我想通过ADS1256将传感器采集的模拟信号转换成数字信号,之后经过SPI口接到MAX3140(SPI转485 chip),再接到MSP430进行数据处理。

    因为我们最终的上位机设备是485的接口。

    这样的话我需要对ADS1256进行编程控制,我得是通过430对其编程吗?您还得有1256的.h文件吧,这个文件也是自己写吗?

    MAX3140是一个SPI转串口的芯片,倒是有SPI接口!