This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

tvp7002不能正常认出水平同步信号

Other Parts Discussed in Thread: TVP7002, THS8135

各位,

我自己做了一块板子,用到了tvp7002,参考的是ths8135 evm的原理图。区别是1,没有使用外部27M时钟;2,没用的引脚都浮空,没用用过电容接地;3,只用到了行,场和绿色信号,没用红色和蓝色信号。

现在我发现芯片能认出场同步,不能认出行同步。不管怎么设置寄存器都不行。从地址0x39,0x3a里读出来的clock per line一直是0。从0x14里面读出来的是0x31,表示没有找到行同步。但是硬件上没有问题,我用示波器看了,管脚上确实有信号。

还有我设置pin22脚为内部参考时钟输出时,有一次有6.7m时钟出来了,但是今天又没有时钟了。