This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GSPS的ADC使用问题,谢谢~

Other Parts Discussed in Thread: LMH6401, LMH6882

1、对于TI的GSPS的ADC,采用两通道I、Q处理架构,每个通道fs。是否可以处理BW=0.8*fs的信号?  是否可以采用零中频?(个人感觉理论上可以)。

2、这种差分架构前端驱动,国半是否有合适的VGA推荐。(不用Balun)。

3、对于Vcmo pin的用法,手册写 “.... For DC-coupled operation, this pin should be left floating or terminated into high-impedance. In DC-coupled Mode, this pin provides an output voltage which is the optimal common-mode voltage for the input signal and should be used to set the common-mode voltage of the driving buffer."这块如何理解,悬空后如何给input供电?

谢谢!