Other Parts Discussed in Thread: LMH6401, LMH6882
1、对于TI的GSPS的ADC,采用两通道I、Q处理架构,每个通道fs。是否可以处理BW=0.8*fs的信号? 是否可以采用零中频?(个人感觉理论上可以)。
2、这种差分架构前端驱动,国半是否有合适的VGA推荐。(不用Balun)。
3、对于Vcmo pin的用法,手册写 “.... For DC-coupled operation, this pin should be left floating or terminated into high-impedance. In DC-coupled Mode, this pin provides an output voltage which is the optimal common-mode voltage for the input signal and should be used to set the common-mode voltage of the driving buffer."这块如何理解,悬空后如何给input供电?
谢谢!