Other Parts Discussed in Thread: ADS1256
请问,若我想通过ADS1256将传感器采集的模拟信号转换成数字信号,之后经过SPI口接到MAX3140(SPI转485 chip),再接到MSP430进行数据处理。
因为我们最终的上位机设备是485的接口。
这样的话我需要对ADS1256进行编程控制,我得是通过430对其编程吗?您还得有1256的.h文件吧,这个文件也是自己写吗?
MAX3140是一个SPI转串口的芯片,有SPI接口!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1256的.h文件当然也是自己写, 可以参考一下官方的说明: http://www.ti.com.cn/cn/lit/an/slaa242/slaa242.pdf
你好,谢谢您的解答!
是这样的:从设备端为(传感器+ADS1256+SPI转485芯片),然后通过modbus总线协议进行485串口通信(485可以一主多从,传输距离也比较远),
总线上只接一个主设备MCU或PC(with software),可以对应多个(传感器+ADS+SPI转串口485单元)从设备,对传感器进行编号,
这样就可以通过一个MCU对个从设备进行控制了。
另:请问ADS1256EVM可以外部输入模拟电流信号(4~20mA)吗?
还有就是外部模拟量的输入电压范围是多少?
谢谢!