1.一直觉得内部基准是2.5V,但是好像是±2.5V?那我是不是只用5V单电源供电,也能够测量负压?
2.采用±2.5V供电时,对于板上的GND,我发现REFOUT是0V左右,但REFOUT和AVSS之间是2.5V这样,所以REFOUT是相对AVSS而言吗?
3.基准电压负端选择,选100(内部基准)时,看框图是直接接在AVSS上的,那么此时我选择内部基准参考电压,可接受输入范围是多少呢?-2.5V到0?还是说Vref = 0-(-2.5V) = 2.5?此时可以测量负压吗?岂不是也不能开PGA?
4.参考电压选择AVDD和AVSS(+2.5V -2.5V)时,可测量范围是多少呢?