Other Parts Discussed in Thread: TLV5636
我用的DA是TLV5636,DA输出的幅值跟参考电压是什么关系??从0至4096调到2048的时候,输出幅值2.68V,再往上输出幅值就调不上去了,芯片的参考电压是2.5V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TLV5636
我用的DA是TLV5636,DA输出的幅值跟参考电压是什么关系??从0至4096调到2048的时候,输出幅值2.68V,再往上输出幅值就调不上去了,芯片的参考电压是2.5V。
TLV5636的输出与否输入输入的关系是Vo= 2 *REF * Din/2^12 Din是12位数字输入, Vo是模拟输出。
但是您要注意的是输出电压受内部运放的限制,最大输出只能是VDD-0.4V, 所以如果你采用VDD=3V,最大输出就是2.6V左右。
TLV5636推荐的REF是2.048V, 因为这样最大输出可以是4.096V, 满足VDD=5V是时VDD-0.4V的输出限制,否则用1.024做基准,VDD=3V时。见datasheet第三页说明:Due to the x2 output buffer, a reference input voltage . (VDD - 0.4 V)/2 causes clipping of the transfer function. The output buffer of the internal reference must be disabled, if an external reference is used.
你好
1、用示波器检查参考电压是否正常;
2、用 逻辑分析仪 或者 示波器,将时钟 、 数据信号捕捉出来,看看发送的数据、时序是否正确。
如果您采用外部参考电压2.5V, 而VDD是5V, 最大输出将是4.6V左右, 您需要注意的是你必须修改配置到外部参考电压,或者您可以选内部2.048V, 看是你的ADC控制是否正常,以及输出是否可以到达4.096V?
The output buffer of the internal reference must be disabled, if an external reference is used. If external reference voltage is applied to the REF pin, external reference MUST be selected.