This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pcm4220过载指示问题

Other Parts Discussed in Thread: PCM4220

我在使用PCM4220进行小批量试制的时候,发现有的pcm4220不能正常指示过载,具体情形如下:

1、当主采样率为8.3886MHz时,采样率为1310572,65536均可以正常显示过载

2、当主采样率为12.288MHz时,采样率为192k,96k等均可能不可以正常显示过载

3、大部分pcm4220可以正常显示,部分不可以。

4、有的芯片一个通道可以,一个通道不可以。

5、测试将mclk降低到11MHz以下,过载显示正常。

6、怀疑采购买的芯片存在质量问题,因此申请了两片样片测试,仍存在不能显示过载的问题。

 

        另,pcm4220配置为24位,left justified,从模式,经典滤波器。

 

请问这可能在哪方面存在问题,急求答案!

电话:0571-88695807   闫工