用于单振元换能器
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,抱歉没有单通道的用于超声波的模拟前端,4通道的AFE5401和AFE5805还是有差别的。
下面是我们超声模拟前端AFE系列的产品选型链接:
4通道的AFE5401和AFE5805有啥不一样,我们是2.5MHz的超声波频率
4通道的5401是差分输入,并且输入端没有TGC,5401主要用于汽车雷达的模拟前端应用。
而5805单端输入,主要用于超声波的应用,所以根据您的应用还是选择AFE5805.
没有集成高压芯片,AFE5805的内部架构如下:内部集成了低噪声运放LNA,电压控制衰减器VCA,可编程增益运放PGA以及低通滤波器LPF。