我在调试AFE58801时选用AC/DC功能时,误将0x07[0]置为1,而0x07[1]为0,但我发现它对我的输出波形有一定的帮助,但是芯片手册上没有给出具体解释,我想知道这一位寄存器的主要功能是什么?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在调试AFE58801时选用AC/DC功能时,误将0x07[0]置为1,而0x07[1]为0,但我发现它对我的输出波形有一定的帮助,但是芯片手册上没有给出具体解释,我想知道这一位寄存器的主要功能是什么?

如下回复:
I checked the internal database and the description of LSB bit of address 0x07 says " Vca i/p clamp voltage inc". So from this description, it seems that this bit adjust the voltage of internal clamp at VCA input.