Other Parts Discussed in Thread: TXB0102
请帮忙推荐自动双向电平转换芯片,需要从1.2V的电平转换到1.2V、1.8V、和3.3V,且需要实现自动双向的GPIO,目前在用的LFS系列有一边的电压必须比另一边的小,不能实现同电压互转,请在帮忙推荐,感谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,目前我们自动电平转换类的芯片只有三种,LSF010x系列,TXS010x系列,TXB010x系列。
TXS和TXB的主要区别在于TXB不建议用于open drain架构的电平转换,比如I2C,建议使用TXSxx系列。
TXSxx系列的电平转换器件,比如TXS0104,TXS0108 我看了下最低电压为1.6V,所以根据您的应用需求,可以考虑使用TXB010x系列,比如2 bit的TXB0102, A port电压范围为
1.2 V ~ 3.6V。B port 电压范围为1.65V~5.5V,VCCA<=VCCB. 所以也可以实现1.2V,1.8V以及3.3V的转换。
您好,是的,如果是1.2V同电平转换,TXS和TXB都实现不了呢。
那么自动电平转换的器件就不满足您的要求了。只能使用带方向控制的电平转换器件了呢。