This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC12DJ800: ADC12DJ800的JESD204B接口

Part Number: ADC12DJ800

使用JESD204B接口,线速率怎么计算?在文档表9-2中线速率等于 fLINERATE=fs*R,如果我选择双通道设备,采样时钟fs为500MHz,在表8-17,中选择模式0,N'=12,M=4,F=8,S=5,R=8,L=4。那按fLINERATE=fs*R=500MHz*8=4G。在其它网上计算线速率公式 Lane Rate=(M*S*N'*10/8*FC)/L=4*5*12*10/8*500/4=37.5G。

  • 您好,关于这个问题,我看下数据手册,稍后给您答复。

  • 您好,抱歉回复晚了。

    参考数据手册Table9-2的例子,JMODE8模式下,4 lanes参考的是Table8-16,R=12.375,fs=800Mhz(4lanes),所以f LINE RATE=12.375*800=9.9Gbps.

    如果我选择双通道设备,采样时钟fs为500MHz,在表8-17,中选择模式0,N'=12,M=4,F=8,S=5,R=8,L=4。那按fLINERATE=fs*R=500MHz*8=4G

    对的,没问题。

    在其它网上计算线速率公式 Lane Rate=(M*S*N'*10/8*FC)/L=4*5*12*10/8*500/4=37.5G。

    我不知道您在其他网上哪里看到的,那么对于ADC12DJ800来说,line rate以数据手册为准。