Part Number: ADS8361
我的目标:四通道差分采样,采样频率为精准的20k(或者20K倍数实现过采样)。
我的问题一:差分采样的模拟输入是否可以0-5V
问题二:可否达到20K的精准采样率
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
首先我想明确一下,您需要四通道同时采样吗?因为 ADS8361内部就集成了两路SAR ADC,不能实现四路同时采样。
ADS8361的转换速率可以到500K,因此可以实现20K采样率,它是通过控制CONVST信号启动转换的,因此采样速率由CONVST信号控制。
我的问题一:差分采样的模拟输入是否可以0-5V
ADS8361的参考电压VREF是2.5V,其输入方式如下截图,需要有输入共模电压2.5V,单端输入的话,负端接2.5V,正端可以接0~5V;
差分输入的话,因共模电压是2.5V,所以每个管脚输入范围是1.25V~3.75V,这样产生±2.5V峰值差分电压,共模电压是2.5V。

问题二:可否达到20K的精准采样率
如上所述取决于CONVST控制信号。
共模电压有个范围,如下截图即2.2V~2.8V,中间值是2.5V:(这是单端的时候,且参考电压是2.5V)

共模电压可以像FIGURE 7 那样加运放电路调节,这是单端输入;差分输入的话,可以选择全差分运放调节,全差分运放一般都有VCOM管脚,即调节输出共模电压的管脚。
我需要的差分共模电压是3.75V,那每个管脚输入范围是2.5V~5V,我这就可以使用。
这样看,您需要采集的信号是共模电压3.75V,差分输入范围是±2.5Vpp。是的,您可以使用2.5V的参考电压,ADS8361满足您的输入要求。