Part Number: AFE5818EVM
Other Parts Discussed in Thread: AFE5818
Hello TI experts
I am using the power supply to power up the AFE5818EVM with 5V (2A) and the LEDs of D2, D1, D3 and D5 on the development board are lit up, and I don't know if this is the normal working condition. In addition, when the development board is powered on, I set the board to the following mode, when there is no analogue signal access, I connect a certain channel to the oscilloscope, it shows a very messy waveform, I would like to ask what is the situation,I hope you can help me!