This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1672: 读出的转换值波动,高7bits无波动,低17bits持续波动,输入0V/2.5V时如图,

Part Number: ADS1672


您好!

最近驱动贵公司ADC芯片:ADS1672, 配置如下:

AVDD=5V, DVDD=3.3V, VREF=2.5V

SCLK_SEL = 1

LL_CONFIG=1

LVDS = 1

FPATH = 1

DRATE0 = 1

DRATE1 = 1

附上测试波形和数据

请帮忙看一下怎么优化可以稳定下来。