This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我使用 TIDA-01022 和两个TSW14J57来验证ADC12DJ3200同步。HSDC PRO使用触发模式,两个ADC之间的相位有时会跳跃一个LMFC周期。这是正常现象吗?
另外,我参考“ TSW14J57revE固件设计文档“并发现TSW14J57不支持基于 sysref 的触发模式。你有可以支持它的固件吗?
请帮忙在英文论坛上问一下,以下为翻译:
Hello, I used TIDA-01022 and two TSW14J57 to verify ADC12DJ3200 synchronization. HSDC PRO uses trigger mode, and the phase between the two ADCs sometimes jumps by one LMFC cycle. Is this a normal phenomenon?
In addition, I refer to the “ TSW14J57revE Firmware Design Document”and found that TSW14J57 does not support sysref based trigger mode. Do you have any firmware that can support it?