如我输出±10V,负载25mA,16通道,则VSS和VCC需要供多少电流,具体功耗怎么计算?根据手册
中ISS和ICC的电流为25mA和-15mA,这个是静态功耗?单个通道需要多少电流,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
VSS和VCC的供电功率需要大于静态功耗加输出功率。
如果您需要输出±10V、25mA的驱动电流,供电电压至少需要±11.5V以上,因为留出1.5V的headroom 和 footroom电压。
负载25mA,16通道,那么输出电流就是25mA*16,输出功率是20V *25mA*16。
静态功耗可以估算为25mA*供电电压。
供电功率除以供电电压就是供电电流。
ISS和ICC的电流为25mA和-15mA,这个是静态功耗?
是的,为静态电流。
单个通道需要多少电流,
不明白您这个问题,每个通道的电流由负载决定,每个通道可以 sink or source的最大电流为25mA。