This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38J84: 芯片的SPI速率,在6.8中提到,典型值为10M,我想知道最低速率能到多少?

Part Number: DAC38J84


我现在的SPI master无法达到10M速率,想知道DAC38J84支持的SPI最低速率是多少?

  • 您好,

    我们的ATE生产在10MHz SCLK下测试器件,因此我们只能确保DAC38J84 SPI总线在10MHz下运行。因此也只给出了这个典型值,没有最大最小值。您若需要以较低的速度使用SCLK,您需要自行测试设备最终性能。

    您描述说“SPI master无法达到10M速率”,具体是什么情况?您有测试波形吗?