This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1291: AVDD-AVSS=4V,他的Vref还能输出4.033V吗

Part Number: ADS1291

请问:

1) AVDD-AVSS=4V,他的Vref还能输出4.033V吗? 供电电压为4V(±2V)对设备有什么影响吗?

2)输入范围计算问题,以2.42V为参考的,差分输入范围最大不应该是0.4V吗,怎么8.3.4.2节说是0.3V,而8.3.4.1节说是0.35V?

  • AVDD-AVSS=4V,他的Vref还能输出4.033V吗? 供电电压为4V(±2V)对设备有什么影响吗?

    AVDD-AVSS=4V的话,即使CONFIG2寄存器配置为4.033V 输出,实际Vref输出也不是4.033V了。

    供电电压为4V的话,设备是能正常工作的,因为AVDD-AVSS的电压范围在2.7V~5.25V时都是能正常工作的,只是数据手册以常用的3V或5V为例做试验得到的电气参数。

    如果为4V的话,内部参考实际输出多少电压要实际测试一下,建议还是使用3V或5V供电方便些。

    输入范围计算问题,以2.42V为参考的,差分输入范围最大不应该是0.4V吗,怎么8.3.4.2节说是0.3V,而8.3.4.1节说是0.35V?

    3-0.2-(6xVdif/2)>CM>0.2+(6xVdif/2)

    2.8-3Vdif>CM>0.2+3Vdif

    当1.25 V < CM < 1.75 V在这个范围内时,当CM=1.75V时,根据CM>0.2+3Vdif<350mV,得到Vdif<350mV ,根据CM>0.2+3Vdif ,得到Vdif<516mV. 取交集Vdif<350mV.

    同样,当CM=1.25V时,根据2.8-3Vdif>CM得到Vdif<516mV, 根据CM>0.2+3Vdif得到Vdif<350mV,同样取交集Vdif<350mV.

    所以可以得到Vdif max为350mV。

    怎么8.3.4.2节说是0.3V,而8.3.4.1节说是0.35V?

    350mV时差分输入最大幅值,而300mV指的是最优的差分输入信号幅值为300mV,不冲突。