Other Parts Discussed in Thread: ADS8860
根据规格书描述AINN可以输入0V,请问在单端应用中,AINN不接缓冲器,直接接地,会不会对精度造成影响?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,ADS8887 数据手册中描述它的输入架构是真差分输入,所以建议使用这款ADC用作差分输入。。
并且给给了INN和INP的满量程范围和输入共模电压范围:
每个输入端的范围为-0.1V~Vref+0.1,差模电压范围为-Vref~Vref,共模电压Vcm= (AINP + AINM)/2.典型值为1/2Vref.

如果您需要单端输入,ANN接地,您可以看下ADS8860,虽然输入也是差分架构,但是可以用作单端输入的应用。