Part Number: DAC38J84
Other Parts Discussed in Thread: TRF3705
DAC38J84的NCO模式,可以调整AB输出之间的相位吗?
如何调整A 和 B 之间的输出的相位?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果您将DAC38J84与射频调制器(即TRF3705)一起使用,则可以将NCO编程为"负频率",并以-180度的方式使用I/Q相位。 然后,您可以看到射频调制器的输出,信号位于射频调制器的本地振荡器的"左侧"或负极侧。
If the user is using the DAC38J84 along with a RF modulator (i.e. TRF3705), then the NCO can be programmed as a "negative frequency" with I/Q phase in -180 degree fashion. The user can then see the output of the RF modulator with the signal on the "left side" or negative side of the Local Oscillator of the RF modulator.