This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38J84: DAC38J84的NCO模式,可以调整AB输出之间的相位吗?

Part Number: DAC38J84
Other Parts Discussed in Thread: TRF3705

DAC38J84的NCO模式,可以调整AB输出之间的相位吗?

如何调整A 和 B 之间的输出的相位?

  • 您好,

    我已将您的问题咨询更了解这款芯片的资深工程师,收到回复后我会同步到这里。

  • DAC38J84具有片上正交调制器校正(quadrature modulator correction ,QMC)电路,用于调整通道A和通道B输出的相位(即相位和正交相位 in-phase and quadrature phase),具体请查看datasheet 如下截图部分:

  • 我现在使用NCO输出,然后我还希望得到一个负的频率?请问这种需要如何实现?是通过调整A B间的相位实现吗?

  • 我已将此问题提交给我们的资深工程师,由于元旦假期,回复将会有所延迟,敬请谅解。

  • 如果您将DAC38J84与射频调制器(即TRF3705)一起使用,则可以将NCO编程为"负频率",并以-180度的方式使用I/Q相位。 然后,您可以看到射频调制器的输出,信号位于射频调制器的本地振荡器的"左侧"或负极侧。

    If the user is using the DAC38J84 along with a RF modulator (i.e. TRF3705), then the NCO can be programmed as a "negative frequency" with I/Q phase in -180 degree fashion. The user can then see the output of the RF modulator with the signal on the "left side" or negative side of the Local Oscillator of the RF modulator.