Part Number: DAC81402
您好,手册Figure7-35提到DAC Output Enable Glitch,sync信号引起的glitch 150mV左右。我使用正负15V提供AVDD,AVSS;DADD 5V,IOVDD3.3V。设计的板卡作为Analogue output,测到了这个glitch。这个glitch影响output输出值比较大。
这个glitch如何减弱直至消除它的影响呢?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,在DACrange 为+-20V范围内,可以看到sync的glitch典型值为0.05V即50mV左右,您现在测试得到150mV,目前测试下来影响输出比较大是吗?
SCLK的jitter大吗? 担心外围电路的影响,比如运放的layout,是否有长的cable连接等?

sync的glitch典型值为0.05V即50mV左右”,是指Figure7-35中sync对应时间(4-5us时刻)的Vou?25us时刻那段的150mV的Vout与这个没有关系?
sync是上面的黑色曲线,可以看到只有在4~5us时刻有glitch,在25us时150mv的噪声是红色曲线Vout。
所以我和您确认是不是sync 的glitch电压测试到150mV,但是从黑色sync曲线来看,最大只有50mV的glitch电压。
4-5us时刻0-5V变化的sync信号会引起Vout信号4-5us时刻50mV左右的变化及25us时刻150mV的变化
您好,我是这么理解的。也就是在DAC output enable glitch的前提下,对比sync和Vout的图,4-5us时刻0-5V变化的sync信号会引起Vout信号4-5us时刻50mV左右的变化。 同时继续观察Sync和Vout的输出,在25us的时候Vout会有150mV的波动,但是这应该不是““4-5us时刻0-5V变化的sync信号”引起的。