This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1:此处的基准电压,REFP实际是0V,REFN是-2.5V,我设计的板子上有生成+-2V5,但不是基准源生成的,是由LM27762产生的,可以直接按照参考电路接入吗?
2:如果不行,请问有没有生成-2V5基准的推荐器件?(我的设计板子上电源条件有:+5V(DCDC),+2v5,-2V5(LM27762产生))
3:我找到一个生成正负2V5基准的器件参考(REF5025&OPA735),但是我板子上只有正5V,正2V5负2V5,没有-5V,请问可以将正负2V5给OPA735供电,5V给REF5025供电,请问电路还能依旧生成负2V5吗?
您好,
1、您是使用±2.5V电源供电是吗?如果是这样的话,REFN管脚才可以输入 -2.5V。
此处的基准电压,REFP实际是0V,REFN是-2.5V
您是需要2.5V的参考电压吗?如果是的话,供电又是±2.5V供电,那么就和datasheet Figure 67一样,建议加REF3125 产生参考电压;
同时建议像 datasheet 中应用一样加OPA350 运放跟随,因为它有瞬态响应能力要求:
2、这个datasheet 截图电路,它是使用的±2.5V供电,AVSS是-2.5V,参考电压输入范围如下截图,它是使用的±2.5V给 REF3125供电然后产生的2.5V 参考电压。
3、我不明白您为什么要生成正负2V5基准?您参考电压实际上需要多少?是2.5V还是5V?
ADS1258 AVDD和 AVSS供电电压是多少?因为AVDD和 AVSS的供电电压限制REFP和REFN管脚的电压,所以我需要了解。
1:我使用LM27762产生正负2V5给ADS1258供电,即给AVDD供2V5,AVSS供负2V5,现在打算参考电压也给正负2V5,正基准2V5我可以使用REF3125得到,我想知道的是负基准2V5我怎样得到,可以直接用LM27762产生的负2V5直接给REFN吗?
2:我待测量的模拟输入信号是在负2V5到正2V5区间的,所以我需要正负电源供电,且基准也同样需要正负基准电压。
3:问题是我如何得到基准电压负2V5,下图的选择是否可以。
3:我找到一个生成正负2V5基准的器件参考(REF5025&OPA735),但是我板子上只有正5V,正2V5负2V5,没有-5V,请问可以将正负2V5给OPA735供电,5V给REF5025供电,请问电路还能依旧生成负2V5吗?
4:此参考电路的REF3125使用的是也正负2v5供电,那输出应该是0V,因为输出是参考接地端的,接地端接的是负2v5,所以就变成了2v5+(-2v5)=0;故参考电路中的ADS1258的引脚REFP接的是0V。且REFN直接接了负2V5,没有使用基准源,是不是可以理解不需要。
REFP实际是0V
1:我使用LM27762产生正负2V5给ADS1258供电,即给AVDD供2V5,AVSS供负2V5,现在打算参考电压也给正负2V5,正基准2V5我可以使用REF3125得到,我想知道的是负基准2V5我怎样得到,可以直接用LM27762产生的负2V5直接给REFN吗?
抱歉我上面误解了您的意思,这样您使用的是5V参考电压。我觉着您可以使用一个产生5V基准电压的芯片就可以了,基准芯片以 -2.5V为参考点。不知道您板子上是否有比5V更高的电压了以用来产生5V基准电压。
使用REF3125的话,我看其datasheet 上有产生-2.5V参考的电路:
但是这个OPA703需要正负电源供电。
2:我待测量的模拟输入信号是在负2V5到正2V5区间的,所以我需要正负电源供电,且基准也同样需要正负基准电压。
输入范围是-2.5V ~ +2.5V的话,您使用2.5V基准电压就够了:
3:问题是我如何得到基准电压负2V5,下图的选择是否可以。
OPA735输出不能完全达到电源轨-2.5V,会有几十mV的gap,因此您需要使用小于-2.5V的电源供电。
4:此参考电路的REF3125使用的是也正负2v5供电,那输出应该是0V,因为输出是参考接地端的,接地端接的是负2v5,所以就变成了2v5+(-2v5)=0;故参考电路中的ADS1258的引脚REFP接的是0V。且REFN直接接了负2V5,没有使用基准源,是不是可以理解不需要。
使用基准源了呀,使用的是2.5V基准,您这里说不需要,具体指不需要什么?
最后,如果您是±2.5V输入范围的话,那么您不需要使用5V参考电压,使用2.5V就够了。
2:我待测量的模拟输入信号是在负2V5到正2V5区间的,所以我需要正负电源供电,且基准也同样需要正负基准电压。
还需要说下,如果这里的正负2.5V是单端输入范围,那么基准电压还是需要5V的,因为差分输入的话就是±5V了,因此需要5V基准电压。
如果这里指差分输入范围±2.5V,那么基准电压选2.5V就够了。
如果需要5V或者说±2.5V的基准电压,您可以在“电源管理”版块咨询下电源工程师,看下根据您板子上现有的电源可以怎样产生。根据我的经验需要需要产生5V电压,肯定需要比5V高的电压源;同样需要产生-2.5V电压,可能需要小于-2.5V的电源,因为电源芯片需要电压降。
1、是输入范围对基准电压的要求,基准电压的大小决定了模拟信号输入范围。因为您使用双电源供电,基准电压的REFN和REFP 管脚其输入电压决定了基准电压的大小,而REFN和REFP 管脚电压的输入范围又与供电电压有关,所以REFN和REFP管脚接入的电压要满足其规格范围。
2、是的,输入范围是±1.06VREF,所以满量程FSR是2*1.06VREF:
1:我看参考原理图Figure67直接接了-2V5进入REFN,没使用基准源产生-2V5,所以问是不是不需要基准源产生-2V5基准电压。
2:参考图的REF3125输出实际是0V对吧,因为它的参考地接的是-2V5。
刚看到漏了这两个问题:
1、我理解可以不需要,ADC供电电源AVSS参考点是-2.5V,基准电压的参考点也是-2.5V,与ADC共地,因此我理解这里可以不需要基准源产生-2V5基准电压。
2、输出多少都是以其参考点来说的,没有参考点没法说其输出多少电压,参考电压是-2.5V,输出是0V,REF3125它实际的功能是将5V(±2.5V)降压到2.5V,这里的参考点是-2.5V。