This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1220: ADS1220和LM7332电路

Part Number: ADS1220
Other Parts Discussed in Thread: LM7322, LM7332,

尊敬的TI工程师,您好:

       如图所示,我需要将4-20ma的传感器输出的电流信号转换为电压信号,然后进入ADC进行采集,我根据模拟工程师手册推荐的使用LM7322运放作为电压跟随器,采样电阻使用150Ω的,LM7322的供电为3.3V,以及ADC的供电和基准电压都使用3.3V,您看电路这么配置是否可以适用

  • 您好,

    首先请注意LM7322和LM7332是不同的运放,它俩输入和输出范围好像都满足要求。

    ADS1220的AGND和DGND要单点连接,更多参考:[FAQ] PCB Layout Guidelines and Grounding Recommendations for High-Resolution ADCs

    您是否打算使用ADS1220 内部集成的PGA?注意看下在enabled PGA 的情况下,输入范围和增益配置是否满足输入范围:

  • 您好,我使用的是LM7332。笔误打错型号,以图片中的7332为准,

    其次,我看到ADS1220的数据手册上写到,对于AINN=AVSS的设置,PGA必须禁用。我图片中打算将输入多路复用器配置为0000,即默认配置,此时AINP=AIN0,AINN=AIN1,

    此时,根据图片中的电路,我将AINN(AIN1)通过一个100Ω的电阻连接到了AGND,那么我是不是应该禁用PGA,并且我的AINN(AIN1)是直接连接到AVSS(AVSS在图中连接到了AGND),还是通过一个100Ω的电阻连接到AGND

  • 是的,AINN=AVSS的话,PGA必须禁用,否则的话不满足输入共模电压要求。

    因为您是输入范围是(4~20)mA *150Ω=0.6V~3V,ADC基准电压3.3V,因此增益只能配置为1,否则话就不满足差分输入范围了。

    您也可以不使用AIN1,配置寄存器1000:

    此时,根据图片中的电路,我将AINN(AIN1)通过一个100Ω的电阻连接到了AGND,那么我是不是应该禁用PGA,并且我的AINN(AIN1)是直接连接到AVSS(AVSS在图中连接到了AGND),还是通过一个100Ω的电阻连接到AGND

    不管您AIN1是否通过100Ω链接AGND,如上所述都需要禁用PGA以满足共模输入范围。

    单端输入的话,建议不使用AIN1,配置多路复用器配置为1000,如上截图,以减少外部走线避免耦合干扰。AIN1直接连接到AVSS也行。

  • 您好,对于我以上给出的原理图,在LM7332的同相输入端需要加入保护电路吗?另外,对于这个电路,其他部分是否有需要优化的地方,感谢您的帮助

  • 对模拟输入的保护一般是ESD和EOS,LM7332内部集成了ESD:

    EOS的话就是电气过应力,就是输入电压超过运放绝对最大额定值:供电电压+0.3V~供电电压-0.3V,有可能发生吗?有可能发生话,就对地和电源加钳位二极管,当然也有弊端就是保护二极管的漏电流会引入失调电压。具体可查看下面ADC系列视频:

    https://edu.21ic.com/video/5092

    另外,对于这个电路,其他部分是否有需要优化的地方,

    没有建议。