This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC083000: 芯片无法正常工作(采数)

Part Number: ADC083000


       当前使用FPGA芯片控制ADC083000工作,FPGA输出的时钟是600Mhz,使用DDR模式接收ADC输出的数据。    

       当前使用的是交流耦合模式。然后通过外部扩展模式(SPI接口)配置ADC083000。当前的状态是,通过SPI接口配置,ADC芯片能进入测试模式。这时FPGA能正确接收到ADC输出的测试数据。但是当模式切回正常的采样模式的时候,FPGA接收到的数据为全FF,且OR一直显示为高。但是此时模拟输入没有加入激励信号。