This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1610量测不稳定

Other Parts Discussed in Thread: ADS1610

请问TI各位

ADS1610量测不稳定是否有debug方向。

ADC校准测试共抓五组数据 ,每一组是100点(固定电压回路100次)的数据,
量回來的值都有一直累加的趨勢,以及亂跳的現象(如:從axxx跳到8xxx又跳到bxxx)。

以下为附档说明:
测试1:电压5V,第一次量。
测试2:电压-5V,测试1量完后接着量,第一笔资料会从测试1最后一笔资料继续累加。
测试3:电压5V,量之前先复位ADC,会从一个新的值开始累加。
测试4:电压-5V,量之前先复位ADC,会从一个新的值开始累加。
试验5:电压2V,量之前先复位的ADC,会从一个新的值开始累加。