Part Number: ADS1256
Other Parts Discussed in Thread: ADS1255
我的ADS1256, 初始化时,关闭了buffer,但是输入通道不接入信号时仍然有0.7V的电压,(此时输入通道通过200K电阻接地), 请问,这是正常的么?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
抱歉,我在邮件中回复,这里没有显示。我再回复一下。

一共配置了4个寄存器: 下面是配置代码
uint8_t buf[4]; /* 暂存ADS1256 寄存器配置参数,之后连续写4个寄存器 */
/* 状态寄存器定义
Bits 7-4 ID3, ID2, ID1, ID0 Factory Programmed Identification Bits (Read Only)
Bit 3 ORDER: Data Output Bit Order
0 = Most Significant Bit First (default)
1 = Least Significant Bit First
Input data is always shifted in most significant byte and bit first. Output data is always shifted out most significant
byte first. The ORDER bit only controls the bit order of the output data within the byte.
Bit 2 ACAL : Auto-Calibration
0 = Auto-Calibration Disabled (default)
1 = Auto-Calibration Enabled
When Auto-Calibration is enabled, self-calibration begins at the completion of the WREG command that changes
the PGA (bits 0-2 of ADCON register), DR (bits 7-0 in the DRATE register) or BUFEN (bit 1 in the STATUS register)
values.
Bit 1 BUFEN: Analog Input Buffer Enable
0 = Buffer Disabled (default)
1 = Buffer Enabled
Bit 0 DRDY : Data Ready (Read Only)
This bit duplicates the state of the DRDY pin.
ACAL=1使能自校准功能。当 PGA,BUFEEN, DRATE改变时会启动自校准
*/
/* ADCON: A/D Control Register (Address 02h)
Bit 7 Reserved, always 0 (Read Only)
Bits 6-5 CLK1, CLK0 : D0/CLKOUT Clock Out Rate Setting
00 = Clock Out OFF
01 = Clock Out Frequency = fCLKIN (default)
10 = Clock Out Frequency = fCLKIN/2
11 = Clock Out Frequency = fCLKIN/4
When not using CLKOUT, it is recommended that it be turned off. These bits can only be reset using the RESET pin.
Bits 4-2 SDCS1, SCDS0: Sensor Detect Current Sources
00 = Sensor Detect OFF (default)
01 = Sensor Detect Current = 0.5 μ A
10 = Sensor Detect Current = 2 μ A
11 = Sensor Detect Current = 10μ A
The Sensor Detect Current Sources can be activated to verify the integrity of an external sensor supplying a signal to the
ADS1255/6. A shorted sensor produces a very small signal while an open-circuit sensor produces a very large signal.
Bits 2-0 PGA2, PGA1, PGA0: Programmable Gain Amplifier Setting
000 = 1 (default)
001 = 2
010 = 4
011 = 8
100 = 16
101 = 32
110 = 64
111 = 64
*/
buf[2] = (0 << 5) | (0 << 3) | (_gain << 0);
//ADS1256_WriteReg(REG_ADCON, (0 << 5) | (0 << 2) | (GAIN_1 << 0)); /* 选择1;1增益, 输入正负5V ,关闭探测电流,关闭clock*/
buf[3] = s_tabDataRate[_drate]; /* 选择数据输出速率 */
CS_0(); /* SPI片选 = 0 */
ADS1256_Send8Bit(CMD_WREG | 0); /* 写寄存器的命令, 并发送寄存器地址 */
ADS1256_Send8Bit(0x03); /* 寄存器个数 - 1, 此处3表示写4个寄存器 */
ADS1256_Send8Bit(buf[0]); /* 设置状态寄存器 */
ADS1256_Send8Bit(buf[1]); /* 设置输入通道参数 */
ADS1256_Send8Bit(buf[2]); /* 设置ADCON控制寄存器,增益 */
ADS1256_Send8Bit(buf[3]); /* 设置输出数据速率 */
CS_1(); /* SPI片选 = 1 */
}
bsp_DelayUS(10);
ADS1256_WaitDRDY(); //
ADS1256_WriteCmd(0xF0); //补偿和增益自校准
bsp_DelayUS(10);
//采集时,先切换通道
ADS1256_WriteReg(REG_MUX, (_ch << 4) | (1 << 3)); /* Bit3 = 1, AINN 固定接 AINCOM ,REG_MUX = 1, */
bsp_DelayUS(5);
ADS1256_WriteCmd(CMD_SYNC); /* CMD_SYNC = 0xFC, Synchronize the A/D Conversion 1111 1100 (FCh) */
bsp_DelayUS(5);
ADS1256_WriteCmd(CMD_WAKEUP); /*CMD_WAKEUP = 0x00, // Completes SYNC and Exits Standby Mode 0000 0000 (00h) */
bsp_DelayUS(5);
ADS1256_WaitDRDY();
//读取采集结果
g_tADS1256.AdcNow[Ch] = ADS1256_ReadData(CMD_RDATA); // CMD_RDATA = 0x01, // Read Data 0000 0001 (01h)