This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC32J25EVM: 使用ADC32J25EVM和TSW14J50EVM进行数据采集

Part Number: ADC32J25EVM
Other Parts Discussed in Thread: TSW14J50EVM, DAC38RF82EVM, LMK04828, DAC38RF82, TSW14J59EVM

专家您好:

我在使用ADC32J25EVM和TSW14J50EVM的过程中,按照指南的步骤进行了操作,但是报错TIMED OUT ERROR,请问您可不可以提供一个详细的设置流程,以便于我们参考进行操作?

另,我的发射端使用的是DAC38RF82EVM以及TSW14J10EVM、KC705,若想要与ADC32J25EVM和TSW14J50EVM完成一个完整的闭环测试,应当如何设置发射端?

希望能够得到一个完整的操作流程步骤,感谢!

  • 您好,关于您的这个问题,我帮您去确认一下。

  • 好的,麻烦您了,期待您的回复

  • 不用客气,这是应该的,我目前还未收到答复,如果收到答复,会立即给您回复。

    给您带来不便非常抱歉。

  • 您好,请问您收到答复了吗

  • 抱歉回复晚了。美国工程师根据您的问题测验复制了现象得到的结论为按照user's guide中的步骤完成是没有问题的。您可以提供下"TIMED OUT ERROR"的步骤?

    另外,对于 DAC38RF82EVM,您是否计划使用 TI IP? 否则、我建议联系 FPGA 供应商、获得有关传输 IP 的支持。 

    I was able to get the ADC up and running with the TSW14J50EVM by following the user guide instructions. Can you please help me understand the steps that were taken to reach the "TIMED OUT ERROR"?

    Additionally, for the DAC38RF82EVM, is the customer planning to use the TI IP? Otherwise, I would recommend reaching out to the FPGA vendor for support with the transmit IP. 

  • 您好,以下是我的具体操作流程:

    1.将DAC38RF82EVM和TSW14J10EVM、KC705相连接

    2.给KC705和DAC38RF82EVM加+5V的电,并将DAC38RF82EVM和TSW14J10EVM与PC相连接。

    3.连接500MHz的晶振到DAC38RF82EVM的J4接口,并确认了JP10处在OPEN的状态

    4.打开DAC GUI,在QUICK START 页面进行如下图的设置,

    然后点击config DAC

    5.LMK04828的Clock outputs页面进行如下设置

    6.打开HSDC Pro,ini文件选择DAC38RF82_LMF_442,并加载。SPS处改为500M。生成单音信号,设置如下

    点击send。

    7.在DAC GUI中点击Reset DAC JESD Core & SYSREF TRIGGER

    8.使用SMA线将DAC38RF82EVM的J6与ADC32J25EVM的J3相连接。

    9.将ADC32J25EVM和TSW14J59EVM相连,供电,并与PC连接。

    10.打开ADC GUI,在Low level界面点击Load config,选择ADC3XJXX_160MSPS_LMK_Setting.cfg并加载,加载后可以看到TSW14J50EVM的D2和D4处于闪烁状态

    11.打开HSDC Pro,选择ADC32JXX_LMF_222.ini.并加载,进行如下的设置

    点击capture,会出现以下弹窗报错

    经确认,D3处于off状态,D4处于闪烁状态、

    以上是我进行操作的全部流程,最终无法正常采集。请您帮忙指出操作过程中的错误或遗漏的操作步骤。

  • 已经将您的操作流程反馈给美国工程师了,如收到回复,会尽快给您通知。

  • 您好,请问有回复了吗

  • 抱歉回复晚了。已经收到回复;您上面提到使用ADC32J25EVM和TSW14J59EVM相连,但是题目中说的是 TSW14J50EVM,所以要确认下使用的是哪个采集板。

    For the ADC32J25EVM, can you please confirm which capture card is being used? You have mentioned both the TSW14J59EVM & TSW14J50EVM.

    Additionally, for the DAC38RF82EVM, is the customer planning to use the TI IP? Otherwise, I would recommend reaching out to the FPGA vendor for support with the transmit IP. 

  • 抱歉,是我输入错误,我使用的是TSW14J50EVM

  • 是我输入错误,我使用的是TSW14J50EVM

    好的。

    for the DAC38RF82EVM, is the customer planning to use the TI IP?

    是打算使用TI IP吗? 

x 出现错误。请重试或与管理员联系。