This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC70502: SPI2C及RSTSEL引脚电平

Part Number: DAC70502


在使用DAC70502设计电压输出设备,为了为使DAC输出达到0-5V,故将VDD电压设置为5.3V,但MCU逻辑电平是3.3V,

现在原理图中将SPI2C和RSTSEL引脚上拉到3.3V电平,是否可行,因为器件手册中的表明要上拉到VDD,

另外SYNC/A0是否也可上拉到3.3V用于设置不同的地址。

3.3V电源会先于5.3V电源上电

  • 现在原理图中将SPI2C和RSTSEL引脚上拉到3.3V电平,是否可行,

    可以的,这两个引脚都是数字控制引脚,高低电平标准如下Vil和Vih的要求,可以看到当大于1.62V时为高电平,当小于0.45V时为低电平,接到3.3V>1.62V  会被认为逻辑高电平。

  • 抱歉,您后面还有这个问题,刚才漏掉了:

    3.3V电源会先于5.3V电源上电

    如果3.3V先于5.3V上电,那么我推荐SPI2C和RSTSEL上拉到VDD,否则的话AVDD还没上电,SPI2C和RSTSEL已经上电,而SPI2C和RSTSEL这两个引脚是在power up期间输出一个有效的电平,如果3.3V先于5.3V上电,不推荐这样接。

    如果同时上电,则接3.3V没问题。