1.您好,我使用ADS仿真了评估板的模拟输入电路,发现S11,S22,S12,参数异常。变压器模型我使用的是从器件官网下载的SNP文件。请问我的仿真电路模型建立的是不是有问题?
2:手册上写的模拟输入接口的阻抗是500欧姆,评估板电路是不是没有做阻抗匹配?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1.您好,我使用ADS仿真了评估板的模拟输入电路,发现S11,S22,S12,参数异常。变压器模型我使用的是从器件官网下载的SNP文件。请问我的仿真电路模型建立的是不是有问题?
2:手册上写的模拟输入接口的阻抗是500欧姆,评估板电路是不是没有做阻抗匹配?
1. 评估板的输入电路在哪里?我在EVM user's guide中没有找到,在数据手册的typical application有参考电路,您说的这个吗?
:
2. 评估板应该是做了阻抗匹配的,手册您指的哪里有描述模拟输入50ohm阻抗?
这里描述的是单端输出阻抗为50ohm。
您好,抱歉,我可能没描述清楚,是差分输入阻抗0.5kΩ,如下图。
2:参考的评估板ADC前端电路是这个(如下图),这个电路中哪部分是起到了阻抗匹配的作用,可以详细解释下吗!
3:(附件是具体的TI评估板原理图文件(www.ti.com.cn/.../sbac155),及我的前端电路ADS仿真文件)
您好,抱歉回复晚了。
是的,单看这个电路,确实没有像平时我们会在差分输入中间端接100ohm电阻,或者在P和N这里即R5和R3这里端接50ohm到地。
EVM这里确使用24.9ohm,我想这里的目的就是为了阻抗匹配,试验验证这样更能获得更好的性能。
或者我的建议是实际layout时,在差分输入端再预留一个100ohm电阻,然后确定是否应在系统评估期间安装该电阻。
好的,我先按照参考电路设计!
1:由手册给出的模拟输入INP,INM上的要求,计算出INP~INM的范围为:2.575~1.625,那么对于评估板电路,我的单端输入接口要如何设置电压摆幅呢?我设置信号发生器的直流偏置为2.1V,VPP摆幅设置为0.95V?,可是这样差分摆幅也只是0.95V啊,手册说的摆幅可以到1.9V。
您好,首先模拟输入端内部已经集成了偏置电路,偏置电压为1.9V。所以不管前端信号发生器的直流偏置电压是多少,建议直接使用AC耦合。
只要保证信号发生器的幅值满足模拟输入电压范围即可。
另外
计算出INP~INM的范围为:2.575~1.625,
这里指的是INP和INM单端的输入范围,也就是单端输入的幅值为0.95Vpp,差分输入的幅值为单端输入的2倍,即1.9Vpp。
所以您只要保证信号发生器的输出幅值给INP和INM为0.95Vpp即可,那么INP-INM的幅值便为1.9Vpp。