This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3663: ADC3663信号输入端口异常

Part Number: ADC3663
Other Parts Discussed in Thread: , ADC3683EVM

ADC3663输入级电路按照手册推荐的方式设计,但没接终端电阻。通过信号发生器给正弦信号,经单端转差分后,示波器测量进入ADC前的信号,发现正弦波变得不规则,有锯齿状缺口。

断开ADC3663信号输入前端的10Ω,发现是ADC3663引起的波形异常,输入端的波形如下:

目前,ADC3663没有进行SPI配置,也没有给时钟。不知为何会这样?严重影响模拟信号的测试,请问大概率是哪里的问题?谢谢!

x 出现错误。请重试或与管理员联系。