新手一枚,现在用到ADS1253,想要获得1M的CLK信号,该如何获得?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢你。有推荐的专用时钟输出芯片吗?
ADS1253是否对该时钟CLK有较高要求?
在ads1251的评估板上使用的是Cypress 的ICD2053BSC-1,你也可以使用这个PLL。
ADS1253对CLK时钟要求并不苛刻,CLK是个施密特触发器形式的输入引脚
如果STM32有CLKO输出引脚是可以的,如果没有,想简单的话可以使用有源晶振,如Crystek 的产品,百度链接如下http://wenku.baidu.com/link?url=VcM94ARqfDyqJEbl-wyaALNobOlG4_IaSXZDRGOjW19kws6R_Ry97CWBxUV9gcSXLfOKCPXU-CToQ7DFK6QO_TrwwX1Irhlw6OJodQQh-HO
你好,想请教你一些关于ADS1253的时序问题。
①:在ADS1253的datasheet上关于图FIGURE 12:Multiplexer Operation。在实际使用中,无法捕捉到T18时刻(约为2043.5tosc的高电平),这个高电平能否捕捉到?
该如何捕捉?
②:当采集4路ADC时,是否是先选择通道,然后捕捉T18的高电平,然后再读取DRDY MODE ,然后读取24位的数据?
非常非常希望能得到你的帮助,谢谢!