Part Number: TLA2024
请问TLA2024 断电后I2C 接口是处于什么状态?客户碰到一个问题,I2C 总线上有接TLA2024 和其他I2C 设备,上拉电阻到3.3V,如果TLA2024 断电,去读另一个I2C 设备的时候,I2C_SDA 电平被拉低,没法到3.3V。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TLA2024
请问TLA2024 断电后I2C 接口是处于什么状态?客户碰到一个问题,I2C 总线上有接TLA2024 和其他I2C 设备,上拉电阻到3.3V,如果TLA2024 断电,去读另一个I2C 设备的时候,I2C_SDA 电平被拉低,没法到3.3V。
根据您的描述,上拉3.3V和TLA2024的电压应该是独立分开的吧?也就是说虽然TLA2024断电,但是I2C上拉的3.3V电压还在,所以这时候主机在读取另一个设备的时候,会被认为总线处于一个被占用的状态。
那如果TLA2024断电,I2C上拉也断开的话,应该就没问题了。
另外,这也涉及到另一个问题,TLA2024断电,如果I2C仍上拉的话,那么sink电流流入芯片端,这里也是要注意的。
您的意思就是2024断电后,主线的电流流入到2024,导致总线电压异常?
不是,我的意思是虽然2024断电,但是I2C仍处于上拉状态,主机在读取另一个2024的时候,会认为总线处于占用状态,因此讲SDA拉低。
另一个问题是2024断电,但是引脚仍有信号(SCL和SDA有电压),那么就会有sink电流流入到引脚,如果超过能承受的最大电流,可能会导致芯片损坏。
这也是我们常说的如果芯片未供电,一些引脚仍有信号出现的问题。