This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

使用ISO7241C隔离SPI信号,在高速通讯时D通道不正常工作

Other Parts Discussed in Thread: ISO7241C

大家好,我在使用ISO7241C隔离两块DSP的SPI信号,一块DSP作为主设备,另一块作为从设备。我发现当我把通讯速度调到4Mbps以上,D通道,也就是SOMI,不能传输正确数据,丢失脉冲。但是其他三个通道工作正常,CLK,CS,SIMO,从设备能收到正确的数据。当通讯速度在4Mbps以下时,主从设备都能收发正确。隔离芯片的连线如下,

CLK  --- PIN 3 (INA)              PIN 14 (OUTA) --- ISO_CLK

SIMO  --- PIN 4 (INB)            PIN 13 (OUTB) --- ISO_SIMO

CS  --- PIN 5 (INC)                PIN 12 (OUTC) --- ISO_CS

SOMI  --- PIN 6 (OUTD)        PIN 11 (IND) --- ISO_SOMI

两侧的EN引脚都连在了本侧的Vcc上,Vcc1和GND,Vcc2和GND之间都连结了0.1uF电容。

是硬件连接方面有问题吗,因为这个隔离芯片的数据手册上写的是25Mbps的最高速度

谢谢!