This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS131A04: 如果AVDD是单电源5V供电,REFEXT不接外部基准电压,只接1uF到地,使用内部基准源4V,是否输入信号范围就只能是0~4V,如果要采集正负2.5V信号,应该如何配置AVDD、AVSS、REFEXT电压,以及ADC芯片的寄存器

Part Number: ADS131A04


关于芯片AVDD和REFEXT基准电压以及信号采集范围,我有两个问题:

1、如果AVDD是单电源5V供电,REFEXT不接外部基准电压,只接1uF到地,使用内部基准源4V,是否ADS131A04采集信号范围就只能是0~4V,如果要采集0~5V信号,是否需要REFEXT外接5V基准电压源,然后AVDD供电不小于5.5V?

如果要采集±2.5V信号,应该如何配置AVDD、AVSS、REFEXT电压,以及ADS131A04的寄存器,能让ADC芯片的电压采集范围和给的数据满足要求。

  • 您好,

    ADS131A04是差分输入接口,如果你需要采集的信号是单端信号,可以采样伪差分形式,如下截图所示:

    差分输入范围是±Vref/Gain,Gain=1,选用内部参考电压4V的话,差分输入范围是±4V,采样单电源5V供电的话,即设置VNCPEN = 0,每个管脚的输入范围是0 ~5V,因此,你可以VAINxN接2.5V,然后VAINxP接0~5V输入,这样差分输入是±2.5V,满足你的采集电压要求。

  • “采样单电源5V供电,设置VNCPEN = 0,每个管脚的输入范围是0 ~5V”,这个我没太理解,如果管脚输入范围变成0~5V,那计算ADC DATA时是按照Vref=5V嘛?还是看那内部参考电压,Vref=4V。

    我看规格书,内部参考电压是4V的话,ADC采集到的1LSB是根据Vref来计算的,我这边实际使用的时候也是发现输入VAINP-VAINN=4V的时候,ADC DATA已经到8,388,607了,输入电压高于4V时,量程因为满了,ADC DATA还是8,388,607,而且负电压量程也只能到-0.5V左右,也没实现±4V。是否是我哪里配置存在问题

  • “采样单电源5V供电,设置VNCPEN = 0,每个管脚的输入范围是0 ~5V”,这个我没太理解,如果管脚输入范围变成0~5V,那计算ADC DATA时是按照Vref=5V嘛?还是看那内部参考电压,Vref=4V。

    按照内部参考电压Vref=4V。0~5V是每个管脚的输入范围,属于单端输入范围。ADC转换的是输入差分电压,差分输入范围是±Vref/Gain。

    我看规格书,内部参考电压是4V的话,ADC采集到的1LSB是根据Vref来计算的,我这边实际使用的时候也是发现输入VAINP-VAINN=4V的时候,ADC DATA已经到8,388,607了,输入电压高于4V时,量程因为满了,ADC DATA还是8,388,607,而且负电压量程也只能到-0.5V左右,也没实现±4V。是否是我哪里配置存在问题

    电路图中你是单端输入,VAINxN你接的是GND,因为差分输入范围是±Vref/Gain,Gain=1、Vref=4V时即是±4V,VAINxP输入范围是0~4V(输入超出4V,不满足差分输入范围),这样造就了差分输入只能是正值,因为VAINxN接的是GND。

    为满足0~5V的输入,你需要VAINxN接2.5V,这样差分输入是±2.5V,在±4V范围内。同时两输入端单端输入范围也满足规格要求,即0~5V。

  • 谢谢耐心指导,我这边再设计一版尝试看看