This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3682: 时钟及控制信号引入

Part Number: ADC3682
Other Parts Discussed in Thread: CDCE6214,

我想使用该款芯片对两路正弦信号进行检测(对地),有一些问题想要请教

1.我看到EVM上有FPGA及FTDI来实现通信,我简单的使用mcu可以实现通信的功能吗,例如STM32?interposer起什么作用,对于mcu还需要吗?此芯片的控制是什么协议?

2.对于时钟源的引入:板上有CDCE6214和外部时钟引入,对于我来说CDCE6214很复杂,有简单的时钟源推荐吗?

3.模拟量的引入:对于我的应用,我认为只需要加一个20M的LPF就可以直接引入输入引脚,您觉得有什么需要注意的吗?

  • 我看到EVM上有FPGA及FTDI来实现通信,我简单的使用mcu可以实现通信的功能吗,例如STM32?interposer起什么作用,对于mcu还需要吗?此芯片的控制是什么协议?

    使用FPGA的原因是因为ADC3682的数字接口是SLVDS接口,使用其他主控也可以,但是通信接口要兼容才可以。

    对于时钟源的引入:板上有CDCE6214和外部时钟引入,对于我来说CDCE6214很复杂,有简单的时钟源推荐吗?

    使用其他时钟源也是可以的,要满足频率和幅值范围,jitter要求,这样才能更好的达到AC性能。CDCE6214是经过试验验证的结果,如果您使用其他的替代 ,建议也是找和CDCE6214的电气参数类似的器件。

    .模拟量的引入:对于我的应用,我认为只需要加一个20M的LPF就可以直接引入输入引脚,您觉得有什么需要注意的吗?

    datasheet P30~32部分讲了很详细模拟前端的设计,包括AC耦合和DC耦合,因为这是一款unbuffer的ADC,所以建议加滤波电路,还要注意滤波电路后也就是ADC输入前的偏置电路,目的是为了保证输入模拟信号满足ADC的输入信号要求,包括共模电压。 建议您参考datasheet中给出的电路设计。