This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC124S021: ADC124S021CIMM在掉电状态下,因VIN输入超过1V损坏

Part Number: ADC124S021

使用如下电路:


在板卡不上电时,外部仍有幅值1V左右的模拟信号到达IN1~IN4时,ADC124S021会损坏。
看ADC124S021的手册描述,有这么一段话:

理解,就算有2V的电压加到IN脚,因为有10K串阻,电流也就0.2mA,远小于10mA的安全值,请教一下,理解的对不对?损坏的原因又是什么呢?

  • 您好,根据note 4这里的提示,您的理解是正确的,这里的意思就是当Vin>VA时,此引脚所能承受的最大电流为10mA可保证器件是安全的。

    并且您通过串联10K电阻防止 出现过电压的应用而是常见的做法,但是目前发现芯片损坏,我想是因为电源可能做出的响应速度不够,不能防范过压信号,也无法吸收这部分电流导致的损坏,您可以尝试在电源端加一个TVS或二极管加以保护试试。