This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7028: ADS7028芯片选型问题

Part Number: ADS7028


尊敬的TI工程师您好:

我们正在选择使用SPI通信、采样频率在1Msps以上的ADC芯片,针对ADS7028芯片有以下两个问题:

1.请问ADS7028芯片的8个ADC通道是否可以同时对模拟信号进行采样?如果可以同时采样,每个通道的采样频率是否均可以达到1Msps?

2.请问有无推荐的微控制器可以与ADS7028搭配?

  • 您好,

    1、不可以同时对8路模拟信号进行采样,ADS7028芯片内部没有集成8个ADC而是1个ADC,它是通过mux进行切换的,如下截图所示:

    2、ADS7028 是 Enhanced-SPI 接口,微控制器带这个接口的都可以,没有特别的推荐,你可以去微控制器板块咨询让微控制器板块的工程师为你推荐。