This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS7884: SPI通信速率要求

Part Number: ADS7884


尊敬的TI工程师您好:

1.在ADS7884芯片的数据表中著有: ,这是否代表着只有当SPI的CS信号拉低时,ADS7884芯片才开始进行采集和转换?

2.在ADS7884芯片的数据表中说明,芯片的最低转换时间和采集时间由VDD引脚电压决定,在VDD电压为5V时,最大吞吐量为3Msps,而每个SPI数据包含16个字节,这是否说明我们的SPI主机时钟频率只能为48M?

3.我们的DSP可以实现12.5M的SPI,我们能否使用此频率的SPI与ADS7884正常通信?(不考虑是否达到最大吞吐量)