您好,我的方波测试信号没有问题,但是实际测量时发现出来的信号都是频率50hz,我的采样频率是500,数据每采集十次就是一个周期,下面是我的采集的波形图,只开启了2通道,
这是否是由于工频干扰过大导致,后续进行50hz滤波能否解决,还是说根本就没有采集到脑电数据,有没有什么解决对策,是哪里出了问题
加了右腿驱动和不加测得的数据都是如此,,,,
下面是我的寄存器配置:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你是否用示波器测量了供电电压的纹波?纹波幅值怎样?
关于GPIOs 配置输入的话不可以悬空,上电默认是配置为输入的:
看你原理图右腿驱动的输出连接在一个2pin接线端子上了,实际是否有连接到人体相应部位?
INxN这些管脚是怎样连接的?
你描述说你开启了2通道,但你寄存器配置只开启了一个通道。你将开启的2个通道的BIAS_SENSP、BIAS_SENSN寄存器位都置1看下是否有改善?
下面文档提到了两种处理50HZ工频干扰的方法,一种是使用RLD 提高CMRR,一种是数据后处理,即在数字域中使用频率为50 Hz或60 Hz的陷波滤波器。
Improving Common-Mode Rejection Using the Right-Leg Drive Amplifier