Part Number: ADS1296R
Other Parts Discussed in Thread: ADS1298R
您好,Ti 工程师!我的ADS1296R芯片的硬件模拟电源电压为± 2.5V,数字电压为3.3V,硬件电压准确,最大纹波为46mvpp,使用内部4V参考源。现在已经测量到外部VREFP引脚也是4V。芯片正常上电时,MCU读取芯片内部电压不准确,偏差较大。寄存器CH4SET I设置的2:0位为011,测得的电压为1.0V,这是不正确的。实际值应约为0.82V。但是我将寄存器CH3SET的2:0位设置为011,测得的电压是正确的,即0.82V。当连接到心电图模拟器时,收集到的波形是混乱和不规则的。请问错误的原因是什么?您是否需要我提供更多参数或原理图?根据ADS1298R的官方参考设计,原理图几乎相同。