This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8695: 微弱光信号检测

Part Number: ADS8695

在设计微弱光检测时进入光电二极管(PD)后产生微弱光电流然后进入跨阻放大等一系列处理后,使用了ADS8695这款芯片作为模数转换芯片,在查看ADS8695手册p58~p59页时看到推荐使用隔离式DC/DC提供电源,包括使用数字隔离器隔离主设备与ADC的SPI通信会带来较好的信噪比以及共模抑制比。

在不考虑电源影响的情况下这里理论计算检测的最小电压只有20mV左右。因此想问如果不采用隔离式的DC/DC,只是通过普通的buck/boost开关电源经过LDO给ADC以及信号处理部分的运放供电会不会有影响甚至说可能达不到设计要求,或者说即使理想情况下能满足设计的水平,那这个系统的比较容易受到干扰造成检测的不稳定。如果说使用这种隔离的电源方案,能不能使检测区分的最小电压更小提高检测精度,如果可以降低电源的干扰从而提高精度是否有比较好的电源方案推荐。