我使用贵公司的ADS1222IPWT,按照其使用手册连线,在面包板上测试时成功;但再重新做了PCB板后,却出了问题:+5V供电,+2.5V参考电压,关TEMPEN,关BUFEN,CLK为2M,SCLK正常,DOUT频率与MUX相同,也就是说无数据输出.AINP2上如连信号-4.5V时,电流增大250mA,但在AINP1上有-4.8V信号,电流却正常.
请帮我分析一下
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我使用贵公司的ADS1222IPWT,按照其使用手册连线,在面包板上测试时成功;但再重新做了PCB板后,却出了问题:+5V供电,+2.5V参考电压,关TEMPEN,关BUFEN,CLK为2M,SCLK正常,DOUT频率与MUX相同,也就是说无数据输出.AINP2上如连信号-4.5V时,电流增大250mA,但在AINP1上有-4.8V信号,电流却正常.
请帮我分析一下
有一个问题需要注意,ADS1222是+/5V差分输出输入,但是对于每一个输入端AINP/N的电压输入范围都是GND-0.1V~~AVDD+0.1V (Buffer off时), 所以不可以负电压输入。