This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC3663: SPI配置管脚电平转换

Part Number: ADC3663
Other Parts Discussed in Thread: TXS0108E-Q1

ADC3663的SPI配置管脚连接至FPGA时遇到IO电平不匹配问题。FPGA的IO是2.5V CMOS电平,ADC3663是1.8V CMOS电平,但是3663的SPI的IO内部有上拉或者下拉21K电阻,目前使用的双向电平转换芯片是TXS0108E-Q1。3663的SCLK和SDIO管脚信号电平不满足要求,会出现类似如下波形:

ADC内部的下拉电阻是无法改变的,所以通过外部上拉电阻调整了电平,但是裕量还是不够。高电平1.5V左右,低电平0.2V左右,ADC无法正常配置成功,有没有更合适的双向电平转换的方案推荐?可以比较灵活的适配ADC内部的下拉电阻。

x 出现错误。请重试或与管理员联系。