读取手册,发现要保证多片AD1278的通道之间相位一致性需要两点:1、CLK一致;2、SYNC_N同时拉高。
我的情况:
1、各个AD1278的CLK来着不同的时钟源,即分别采用10ppm的30MHz时钟通过FPGA内部的PLL产生25.6MHz时钟。
2、两个AD1278的SYNC_N信号大约有200ns的时延差;
问题:
两个AD1278之间的相位差120us?为啥有这么大的相位差?谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
读取手册,发现要保证多片AD1278的通道之间相位一致性需要两点:1、CLK一致;2、SYNC_N同时拉高。
我的情况:
1、各个AD1278的CLK来着不同的时钟源,即分别采用10ppm的30MHz时钟通过FPGA内部的PLL产生25.6MHz时钟。
2、两个AD1278的SYNC_N信号大约有200ns的时延差;
问题:
两个AD1278之间的相位差120us?为啥有这么大的相位差?谢谢!!!
现在对数据的分析显示:误差约有40us(差2个采样点),ps:上个帖子是120us,管脚设置给错了;
问题是FPGA的PLL输出的采样时钟会有这么大的影响吗?
1、这个ADC的前端采用64倍的放大输入,信噪比足够大
2、同一个CLK来驱动ADC,没有问题,两个片子的两个通道之间的相位差很小;
3、我现在是两块板子的ADC,采用的CLK是不同的晶振,频率都是30MHz通过FPGA的PLL转为25.6MHz
4、新发现的问题,两块板子之间的ADC的相位差还会随时间变化?导致我的疑惑的是这样想延时补偿都没有办法?
5、对这个ADC而言,我个人理解主要的控制信号是SYNC_N、CLK、FSYNC、PWDN_N;我FPGA程序启动的顺序为:PWDN_N->CLK->FSYNC\SYNC_N